EH-20 (Base model only) Missing Hardware Kits

Issue

Missing hardware kits in the base model of the EH-20 unit

Product Line

Pelco Cameras

Environment

EH-20 Base only Model 

Cause

Customer opens up box and no hardware kit is inside

Resolution

Will need to contact tech support 1-800-289-9100

Kit includes:

Qty:2 1/4-20 X.375-inch Screws for the sun shroud mounting

Qty:2 1/4inch nylon flat washers for the sun shroud mounting

Qty:1 1/4-20 X.37-inch screw for camera mounting

Qty:1 1/4inch lock washer for camera mounting

Qty:1 1/4inch steel flat washer for camera mounting

Qty:1 T30 Torx wrench