Using Multicast Hammer

Issue

Multicast Hammer

Product Line

Pelco Video Management

Environment

VMS

Cause

Multicast Network Issues

Resolution

Download Multicast Hammer v2.1 here

Client Settings;

 

Server Settings:

- Set the Transmit Speed to 500 Mbps when testing multicast between Server and Client devices.  Anything over this threshold will likely cause loss on almost any 1 Gbps Port
- Set the Payload Bytes to 1400
- Set the Burst Packets to 1