Sigma and Windows 10

Issue

Does Sigma run on Windows 10

Product Line

Satchwell Sigma

Environment

Sigma

Windows 10

Cause

Is Sigma 4.08 supported on windows 10.

Resolution

No version of Sigma is supported on a Windows 10 platform except:

Sigma 4.08 can only be installed on Windows 10 when the software is used as a transition into EcoStruxure Building Operation ( EBO ) and used with the correct version of transition component.

 

For full details of Sigma 4.08 versions, build no's and operating systems supported click here.