BU-ADAPTER Missing 4 flat head screws

Issue

Manual shows BU-ADAPTER should come with 4 Flat head screws

Product Line

Other, Pelco Cameras

Environment

BU-ADAPTER

Cause

Manual is incorrect for the BU-ADAPTER shows 4 flat head screws included and should read not supplied.

Resolution

This will be fixed when the next manual is updated. The 4 flat head screws are customer supplied and not supplied from Pelco.  This is because we don't know what size of Conduit Box the adapter plate will be mounted too.

 

 

These are the screws kits that come in the BU-ADAPTER KIT BOX

 

This is the BU-ADAPTER plate