Digital Sentry: What PTZ keyboards are supported with DS ControlPoint?

Issue

The KBD300a is no longer sold by Pelco, what keyboards can be used instead?

Product Line

Pelco Video Management

Environment

  • Digital Sentry
    • DSSRV / DSSRV2 / DS NVs
    • DS ControlPoint client
  • KBD300a joystick
    • Obsolete and no longer sold
  • KBD5000 / 3D Mouse
    • The current supported PTZ keyboards for Digital Sentry

Cause

The KBD300a is no longer available for purchase.

Resolution

Third party keyboards are not supported with Digital Sentry / DS ControlPoint.


Digital Sentry supports the following two keyboards: 

  • KBD5000 
     
  • Enhanced 3D Mouse
     
  • KBD300a (This keyboard is no longer sold but could still be in use)

 

KBD5000


 

Part Number = KBD5000

KBD5000 Keyboard Specification Sheet (when used with an Endura VMS)


Configuration information with DS ControlPoint, refer to KBD5000 Setup and Configuration with DS ControlPoint    


 

Enhanced 3D Mouse


 

Part Number = 3DX-600-3DMOUSE


Configuring information with DS ControlPoint, refer to 3D Mouse Operations Guide for DS ControlPoint   

 

 

KBD300A

**No longer sold and is Obsolete

Configuration information with DS ControlPoint, refer to How to connect a KBD300A to a DSSRV / DSSRV2 or Client PC running DS ControlPoint and what are the functions?