Increasing Size of PCT Project folder Issue

Issue

PCT project folder size increases when an object is deleted.

Product Line

SmartStruxure Solution, Other

Environment

Project Configuration Tool, PCT

Cause

Any change made in PCT increase the size of PCT project folder. This is a normal behavior of PCT.

Resolution

Users can create a new project and restore the backup of ES or AS from the current project to reduce the folder size.