Digital Sentry: Adding an Axis P3707 to a DS recorder.

Issue

Adding the Axis IP camera using the ONVIF driver results in only one video channel discovered.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry
    • DSSRV / DSSRV2 / DS NVs
  • Axis P3707-PE

Cause

Unsupported model

Resolution

The camera needs to be added manually using the RTSP streams.


The RTSP stream URL which can be used per the AXIS P3707 user manual

Text File with the links to copy if needed
 

Use this KB article to understand the process on how to manually add a camera to DS using the RTSP stream URL: http://buildingskb.schneider-electric.com/view.php?AID=14179

Refrence: Axis P3707-PE user manual