EH20 Heater and Fan Turn on and off Temperatures

Issue

Nothing listed in the Spec sheet for the Temperature when the heater or fan comes on for the EH20 enclosure.

Product Line

Other, Pelco Cameras

Environment

  • EH20-2-H
  • EH20-3-H
  • EH20-P-H

Cause

No Documents showing when the Heather or Fan comes on in the EH20 series enclosure.

Resolution

The Heater turns on at 5 Celsius or 41 Fahrenheit

The Fan comes on at 34 Celsius or 93.2 Fahrenheit

The Heather turns off at 10 Celsius or 50 Fahrenheit

The Fan turns off at 30 Celsius or 86 Fahrenheit