This Xbuilder project requires the domino platform version to be >= 2.6.0 error when trying to download project to a Xenta 511/527/913.

Issue

"The Target System is of an old version.
This Xbuilder project requires the domino platform version to be >= 2.6.0"

Product Line

TAC I/NET, TAC Vista

Environment

  • XBuilder version 1.5.0
  • Xenta Server
  • Xenta 511, 527, 913

Cause

This error is caused by trying to download to a Xenta 511/527/913 that is not running the compatible system program for Xbuilder version 1.5.0.

Resolution

Upgrade the device according to the following chart to correct this:
 

Xenta Unit Version
511 2.3.0
527 1.1.0
913 2.0