HID Proxpro with keypad

Issue

HID Proxpro with keypad

Product Line

TAC I/NET, Andover Continuum

Environment

Applies to both I/NET and Continuum door controllers.

Cause

Information pertaining to the HID ProxPro  

Resolution

When ordering a keypad reader from HID, you need to make sure the Configuration Setting option is "09 - Buffer one key, add compliment, 8 bit message (Dorado)".

Example: 5355 AGK 09 - ProxPro w/ Keypad

If you are using the 5535 model reader on an Infinity ACX781 or ACX780 model controller you will need to order with Configuration Setting option 00.