Issue
Battery Back up for MIPs and Controllers
Environment
I/NET site
Cause
Explaining the Battery Back up for MIPs and Controllers
Resolution
Controllers that are using MIPs like the 7700 series, once added to the baseboard now holds the database and it is backed up by the battery on this card. The onboard battery is now used only for clock power. MIPs on the taps however do not, since they only hold the Bin file for the respective types and no save file or database.