Issue
What is "Verbose" within Vista Server Setup?
Documentation refers to "certain dialogs and messages." What are these certain dialogs?
Product Line
TAC Vista
Environment
- TAC Vista Server Setup
- TAC Vista Workstation
Cause
The documentation states that this setting: "Enables or disables the display of certain dialogs and messages for operator communication."
Resolution
Verbose turns on questions that ask if you really want to do something. An example, "Do you really want to quit?" when closing Vista server.