Issue
What does "Commence Communication" do?
Environment
- LonMaker
- TAC Vista System Plug-In
Cause
The menu option in the System Plug-in to commence communication is a common troubleshooting step. Understanding exactly what occurs when this option is selected is beneficial to know when it will be helpful.
Resolution
The function of "Commence Communication" is to upload the Vista group and configuration parameters to the Vista database. When creating a new network, it is necessary to execute the "Commence Communication" command as the final step of the process.