Issue
Entering values less than 1 in Zbuilder results in red error indication. If you enter ".05" or ".2" into a field in Zbuilder it won't accept it.
Environment
- Zbuilder
- Xenta 121
Cause
A period cannot be the leading digit in a numerical input.
Resolution
The first digit must be a number, so you must enter fractional values with a leading zero. Example: "0.05" or "0.2"