Issue
Trying to filter alarms on Vista Workstation 4.5.
Is there a way to permanently set the filter to only display alarms with a priority of 1-8?
Environment
Vista Workstation 4.5
Cause
Permanently setting alarm filters allow for creation of custom alarm views.
Resolution
In Vista 4.5 you can create user profiles, and assign a custom alarm view to the profile.
For more information on how to set up user profiles and alarm viewers see the "TAC Vista IV, Administrating TAC Vista Workstation" manual. If no profile is specified for a user it will use the global object $UserProfile which uses the global object $AlarmView. If you make changes to those objects it will affect all users that are not using their own profiles.