Do not configure HTTP and HTTPS on the same port of a Xenta 511/527/913

Issue

Warning: Configuring HTTP and HTTPS on Xenta 511/527/913

Product Line

TAC Vista

Environment

  • Xenta 511
  • Xenta 527
  • Xenta 913

Cause

If the device reboots with both protocols set to the same port then it will become stuck in an endless reboot. The only way to correct this problem is to send the device back to the factory.

Resolution

When configuring the HTTP (80 by default) and HTTPS (443 by default) ports in the Xenta 511/527/913 do not try to set these two protocols to use the same ports.