Issue
Change the LED pattern on card readers
Environment
Continuum Site
Cause
How to Change the LED pattern on card readers
Resolution
On the ACX line of Infinet controllers and also the AC1+ modules you can change the dynamics of the reader LED.
The Alternate LED pattern is selected by creating a numeric point whose name is AccessLEDPattern. When this point exists, the Alternate LED pattern will be employed by the access controller. When this point does not exist, the standard LED pattern will be employed. It should be noted that cold-starting or resetting the access controller does not delete or destroy the AccessLEDPattern.