Issue
If a widescreen monitor is used, graphics will display properly in Vista, but if you open them for editing in Graphics Editor, they appear stretched horizontally. Conversely, if you create a graphic in Graphics editor that looks proper, it will appear to be squished horizontally in Vista, and the alignment of any text will be off.
Environment
Vista IV OGC Graphics Editor
Cause
The computer being used has a widescreen primary display.
Resolution
Resize the primary widescreen display to a resolution with a 4:3 aspect ratio, 800x600, 1024x768, etc. or, if a secondary display with normal aspect ratio is also connected, it must be set as the primary display.