How do I set up a point on a graphic page to do Automatic Page Display

Issue

How do I set up a point on a graphic page to do "Automatic Page Display"

Product Line

TAC I/NET

Environment

I/NET Site

Cause

How to set up a point on a graphic page to perform an "Automatic Page Display

Resolution

  1. Open a graphic page in the “Edit Mode”
  2. Select the point that you want to trigger that page and do a right mouse click
  3. Select the properties option

Note: I/NET can have up to seven system pages displayed at one time. Each time an incoming alarm causes a new page to display, the new page will appear in front of previously displayed pages.

System pages are displayed behind any open editors and summary windows. You will have to close these windows in order to view the displayed system pages. Because system pages may be hidden by other windows, you may wish to also configure an audible alarm for the point.