Issue
Limitation of Groups/Units in one Vista DB
Environment
- Vista database
- Xenta groups
- LonWorks groups
Cause
Network design limitations, maximum number of controls used on a network.
Resolution
- No more than 30 TAC Xenta groups per LonTalk Adapter.
- No More than 30 TAC Xenta base devices per TAC Xenta group.
- Maximum of 400 TAC Xenta base devices per LonWorks network
- No more than 50 LonWorks groups per network.
- No more than 64 LonWorks units per LonWorks group.
- Maximum of 1000 Devices using standard SNVT communications.