Issue
LonMaker repeatedly prompting to drop items on a resynchronize command
Environment
Echelon LonMaker
Cause
When LonMaker resynchronizes there is an option that is sometimes overlooked to "Automatically add shapes to drawing." If this is unselected then the process may take a very long time to fix the drawing of large networks because of the manual placement of shapes.
Resolution
Select "Automatically add shapes to the drawing" in the Resynchronize prompt to avoid manually placing each new shape.