How to create a link to an Alarm/Eventview in a TAC Vista graphic (OGC).

Issue

How to create a link to an Alarm/Eventview in a TAC Vista graphic (OGC).

Product Line

TAC Vista

Environment

  • TAC Vista IV
  • OGC Graphic Editor

Cause

This feature is really good if you have multiple sites in the Vista database and need to access events or alarms from one site from your graphic.

Resolution

  1. In Graphic editor, create a link area.
  2. In the link area, browse other graphics. You can also manually write a path to an object.
  3. Write the path to your Event or Alarmview object
  4. Save the graphic to database
  5. Close the editor.
  6. Open the graphic in Vista Workstation, click on the link area and your personal alarm view will appear.