Issue
How to tell if an AC-1 Plus card reader has been tampered with
Environment
AC-1 Plus card reader
Cause
Knowing whether a card reader has been tampered with is an important security measure.
Resolution
- Set up an InfinityNumeric. Name it anything.
- Set its IOU number the same as the entry IOU (or exit IOU) of the door and set the channel number to 6.
- Set the direction for IOInput.
-
The value of the numeric represents the status of the reader.
- 0 = Normal
- 1 = No Reader Present
-
2 = Reader Voltage problem
NOTE: This only works on the AC1Plus access control module.