Issue
Error message "Exception from HRESULT: 0x80041038 Code: -2147217352" when logging into TAC Vista Webstation 5.0.0
Environment
- Webstation 5.0.0
- Internet Explorer
Cause
This error results from an attempt to log in with an invalid user/password
Resolution
Check that the username and password are valid and try to log in again.