A BACnet Binary Input object cannot be added to a Niagara R2 container.

Issue

A BACnet Binary Input object cannot be added to a Niagara R2 container.

Product Line

TAC I/A Series

Environment

Workplace Pro

Cause

In Workplace Pro, BACnet objects must be placed under BACnet devices.

Resolution

  1. Copy a BACnet Device from the Local Library (/tridiumx/BACnet/objects/BACnetDevice) into the container
  2. Add the BACnet object under the device.
  3. For more information, refer to the BACnet Integration Reference.