Issue
A Niagara R2 station listed under localhost won't open. In the fui.exe console window, this message appears:
Requestclient.handshake [serverSessionId=3]
Station=josh [0] Station
The station never opens.
Environment
Niagara R2 station
Cause
This behavior is caused by McAfee Security Centers Proxy Service.
Resolution
Disable the proxy service and reboot the computer. Follow the steps below to disable this service:
- Open the Windows services - (Click on Start - Run - then type service.msc)
- Scroll down to the McAfee Proxy service.
- Disable this service by right-clicking on the service - select properties - change the startup type to disabled.
- Reboot the computer.
This should allow the station to run correctly on the localhost.