When using Workplace Tech, links won't create between two objects. No matter what type of objects, the link line remains red and the application will not link the two objects.

Issue

When using Workplace Tech, links won't create between two objects.  No matter what type of objects, the link line remains red and the application will not link the two objects.

Product Line

TAC I/A Series

Environment

Workplace Tech

Cause

In Microsoft Visio, the Snap & Glue feature is disabled.

Resolution

 To enable Snap and Glue go to Tools > Snap & Glue, then check the Snap box and the Glue box.