Issue
Will Niagara R2 and G3 applications (ie: Workplace Pro, Workbench) run on a dual-processor/dual core/duo laptop?
Environment
- Niagara R2
- Niagara G3
- Workplace Pro
- Workbench
- Dual core processor PC
Cause
As per Tridium sales and technical support, both applications will run on dual processor computers, though they have not been specifically tested.
For more information on Workplace Pro review document F-26999 and for more information on Workbench review document F-27426.
Resolution
Minimum hardware requirements for Niagara applications are as follows:
- R2 - Workplace Pro: Intel Pentium IV 1GHz processor, 512 MB RAM, 1GB hard disk space
- G3 - Workbench: Intel Pentium IV 2GHz processor, 1 GB RAM, 1GB hard disk space