How can the Niagarad service for Niagara G3 be started?

Issue

How can the Niagarad service for Niagara G3 be started?

Product Line

TAC I/A Series

Environment

  • Niagarad service
  • Niagara G3

Cause

There are three different ways to start the Niagarad service manually.

Resolution

  1. From the Windows Start menu: click Programs > Vykon AX Supervisor 3.x.x > Install Platform Daemon
  2. Open a DOS window and type - cd\Niagara\Niagara-3.x.x\bin then type plat.exe installdaemon
  3. Create a desktop shortcut with the following: C:\niagara\niagara-3.x.x\bin\plat.exe installdaemon