Issue
When using Link Builder in the WorkPlace Commissioning Tool, a change to the COV Client Subscription Lifetime to large minute increments (i.e. 60 minutes), is rejected.
Environment
WorkPlace Commissioning Tool
Cause
Incrementing the current values in large minute is known to create an issue, implement the below work-around to increase the lifetime value.
Resolution
The work-around for this issue is to change the COV Client Subscription Lifetime from its current value to the next incremental value (up one minute) and then to the desired value (i.e. 60 minutes).