Issue
Getting error 'Failed to access IIS' when starting webstation.
Environment
TAC Vista Webstation
Cause
This happens if IIS is installed before .NET Framework.
Resolution
It is necessary to register ASP.NET with IIS.
- From the Windows Start Menu>Run
- In the Run window type "cmd" to open the command prompt window
- To register ASP .NET 2.0, In the command prompt window, type "%windir%\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i"
- To register ASP .NET 4.0, In the command prompt window, type "%windir%\Microsoft.NET\Framework\v4.0.30319\aspnet_regiis.exe -i"
This command will re-register ASP.NET as if it were installed after IIS.