Issue
When starting SIGNAL for Windows XP, an error message appears stating "Can't run 16 bit Windows program, insufficient memory". This occurs when the SIGNAL program "Startup Type" is set for Automatic.
Environment
SIGNAL for Windows XP
Cause
Multiple versions of SIGNAL for Windows XP are trying to run simultaneously. The “active” user profile, as well as, the “All Users” profile are both trying to start SIGNAL.
Resolution
When it is required to have SIGNAL startup automatically for ALL users, either make the entry for each user profile or only make the entry in the “All Users” profile.