SIGNAL (any version) is installed on new computer hardware that has higher video resolutions. Now, the Monitor program’s graphics are not aligned.

Issue

SIGNAL (any version) is installed on new computer hardware that has higher video resolutions. Now, the Monitor program’s graphics are not aligned.

Product Line

TAC I/A Series

Environment

  • SIGNAL (all version)
  • PC with high resolution graphic card

Cause

The new PC screen resolution is not set at the recommended resolution.

Resolution

All versions of SIGNAL support two video resolutions: 640 x 480, and 800 x 600.

Shutdown SIGNAL and use Windows to modify the computer’s video resolution to one of these two settings.