Issue
Receiving error “Could not connect to server. Cause: System.Runtime.Remoting.RemotingException:Requested Service not found opening graphics in webclient
Environment
Windows XP
Windows Server 2003
Windows Server 2008
Cause
This issue usually happens after uninstalling and reinstalling IIS.
The webclient and newgraphicsfiles virtual directories may have been added, but DNWACServerFactory was not.
Since the DNWACServerFactory virtual folder is missing, it keeps trying to create itself, but it can't and it generates the error.
Resolution
- Get all users out of webclient
-
In IIS (Internet Information Services Manager)
Right click on Default Web Site, select New> Virtual Directory
Click Next -
In the Alias field type: DNWACServerFactory, Click Next
Click Browse and navigate to C:\Progam Files\ Continuum\DNWACServerFactory
Click Next -
For access permissions, keep read, run scripts and select browse
Click Next, Click Finish - Restart webclient and test out graphics