XBuilder crashes when a LNS network is inserted

Issue

XBuilder crashes when a LNS network is inserted

Product Line

TAC Vista

Environment

  • XBuilder
  • LNS Network

Cause

XBuilder will crash when a LNS network is inserted that contains a XIF file which has multiple signals with the same name.

Resolution

If Vista 5.0.0 or higher is being used you can create a Vista database solely for the purpose of inserting it into XBuilder to avoid this problem.

Otherwise the XIF file will need to be modified to remove the duplicate names and the template replaced with the new XIF file.