Issue
How can BACnet objects be learned as "full" objects and not "lite" objects in Niagara R2?
Environment
Niagara R2
Cause
"Use lite objects" is enabled and need to be disable (uncheck the box) "Use Lite Objects" setting using BACnet Utilities.
Resolution
From the BACnet Utilities window, when performing either a "network - learnNetwork" or "device - learnDevice" command, clicking the Execute button will generate a pop-up window. In this window, uncheck "Use lite objects", and click OK to proceed.