Issue
Registering RVCTL.DLL Video
Product Line
TAC INET
Environment
- DVR Servers
- RVCTL.DLL
- CCTV
Cause
This video will illustrate how to install the RVCTL.DLL files on your PC. The RVCTL.DLL files are no longer installed automatically.
Resolution
The old and new RVCTL.DLL files are located in a folder within the support directory on the installation CD. To start, go to CD > Support > and select the RVCTL.DLL folder. Open the RVCTL.DLL text file and follow the instructions on it. This will install your files and allow your DVR to function properly with I/NET.
- Determine which rvctl.dll is required.
- Copy the files from the CD folder Support\RVCTL\"Your version folder" into the INET Seven root folder at X:\Program Files\INET Seven; where X = the windows os
- Open a cmd prompt. User Start > Run, type cmd and select OK
- Type the following:
cd\ <cr> cd Program Files\INET Seven <cr> regsvr32 rvctl.dll <cr>
You will see a message box with the message DllRegisterServer in rvctl.dll succeeded. The rvctl DLL is now registered and can be used for Integral DVR servers to INET.