Issue
The following error appears in the Niagara R2 UNC Standard Output Window:
Duplicate Server Sessions - kill (Enterprise Server Name).
Environment
Niagara R2 UNC
Cause
Running multiple R2 stations can cause issue with the subscription of the UNCs in the address book of the Enterprise Server station.
Resolution
An Enterprise Server has the ability to run multiple R2 stations at one time. Under normal circumstances only one station should be running on a server.