Is there a way to use Points in I/NET Seven to calculate the Heat Index the Weather person uses in their forecast?

Issue

Is there a way to use Points in I/NET Seven to calculate the "Heat Index" the Weather person uses in their forecast?

Product Line

TAC I/NET

Environment

I/NET site

Cause

Desire to use HEAT INDEX information

Resolution

Yes you can determine the "Heat Index" within I/NET Seven. The only External points required are the following:

  1. Outside Air Temp sensor
  2. Outside Air Rh sensor

Please see the attached Word doc that shows the Calculations involved to determine the "HI"

Word doc "What is Heat Index"

What is Heat Index