What are the current versions of PSI and related programs?

Issue

What are the current versions of PSI and related programs?

Product Line

TAC I/A Series

Environment

Network 8000

Cause

Software tools for Network 8000 devices

Resolution

The latest version of the PSI software is PSI v4.10. It can be downloaded from The Exchange Download Center.

This release contains a software bundle consisting of 8 different PSI tools including:

  • MicroZoneII (MZII)
  • MicroFlow II (MFII)
  • MicroFlow II Air Balance (MFII-Air Balance)
  • LIM
  • PEM
  • XPSI
  • MicroNet-CI (MNet-CI)
  • MicroNet-CI Air Balance (MNet-Air Balance)