Issue
Changing the NetController Model Type between 9900 and 9940
Environment
- NetController CX9900
- NetController CX9940
Cause
Update NetController model number in Continuum database
Resolution
- Backup the database.
- Shut down Continuum as precautionary measure
- Open the SQL Enterprise Manager
- Open the SQL Query Analyzer
- Select the ContinuumDB
- To change from 9900 to 9940, type in update infinitycontroller set CntrlType = 44 where UiName = ‘Infinity1’ and execute
- To change from 9940 to 9900, type in update infinitycontroller set CntrlType = 42 where UiName = ‘Infinity1’ and execute
- Please note that you must change ‘Infinity1’ to match the Uiname of your controller
- Start Continuum up again and verify that the change was effective