Door Force Lock schedule configuration

Issue

Door Force Lock schedule configuration

Product Line

Andover Continuum

Environment

Continuum Access Control

Cause

Enable the Door Force Lock Schedule attribute in the Door object.

Resolution

Door Force Lock schedule configuration

This is a two part setting in order to successfully make Door Force Lock schedule work.

If you set up a point in the Door Force Lock Schedule on the options tab, You will need to check either Normal and/or Comm Fail
on the entry reader tab of the door editor in order to successfully work.