Issue
UltiVist/NETWORK 8000, how to remove all or parts of the E: Segment.
Environment
NETWORK 8000
Cause
Procedure on removing a segment.
Resolution
KILBRNCH is a powerful tool, before doing the following procedure, BACKUP THE DATABASE.
In an OS/2 window, go to the FI directory and type SET NOFCS=TRUE (this command turns off communications so that the KILBRNCH command will only delete the elements in the E: Segment set to 'offline'). Press Return.
After getting the x:\FI prompt back, type KILBRNCH FI
After completion, go to FI directory and then type SET NOFCS=FALSE. Refresh the E: Segment.