Issue
Vista 5.0.3 Graphics Editor crashes when you right-click on a graphics page in Workstation and click edit.
Here is the error message:
Could not load file or assembly 'TAC.Interop.TacosOI, Version=5.0.0.0, Culture=neutral, PublicKeyToken=null' or one of its dependencies. The located assembly's manifest definition does not match the assembly reference. (Exception from HRESULT: 0x80131040)
FileLoadException
at TAC.Graphics.Windows.Vista.VistaSystemProxy.Create(String server, String user)
at TAC.Graphics.Editor.EditorApplication.CreateApplicationForm(ReadOnlyCollection`1 commandLine) in C:\TAC\VistaSw\V5030\Graphics\Editor\EditorApplication.cs:line 90
at TAC.Graphics.Editor.SingleInstanceApplication.<>c__DisplayClass3.b__1(Object splashFormSender, EventArgs splashFormEventArgs) in C:\TAC\VistaSw\V5030\Graphics\Editor\SingleInstanceApplication.cs:line 79
at System.Windows.Forms.Form.OnShown(EventArgs e)
at System.Windows.Forms.Form.CallShownEvent()
at System.Windows.Forms.Control.InvokeMarshaledCallbackDo ThreadMethodEntry tme)
at System.Windows.Forms.Control.InvokeMarshaledCallbackHelper(Object obj)
at System.Threading.ExecutionContext.runTryCode(Object userData)
at System.Runtime.CompilerServices.RuntimeHelpers.ExecuteCodeWithGuaranteedCleanup(TryCode code, CleanupCode backoutCode, Object userData)
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
at System.Threading.ExecutionContext.Run(ExecutionContext executionContext, ContextCallback callback, Object state)
at System.Windows.Forms.Control.InvokeMarshaledCallback(ThreadMethodEntry tme)
at System.Windows.Forms.Control.InvokeMarshaledCallbacks()
Environment
Vista Workstation 5.0.3
TAC TGML Graphics Editor 1.0.3
Cause
An error occurred at installation and the Graphics Editor must be removed completely and reinstalled.
Resolution
- Shutdown the Vista Server and Workstation.
- Uninstall the TAC Graphics Editor 1.0.3 from the Control Panel of the PC.
- Delete the entire C:\Program Files\TAC\GraphicsEditor directory that is left behind from the un-install.
- Download the TACGraphicsEditor103.exe from The Exchange.
- Re-install the TACGraphicsEditor103.exe