Installing TAC Vista 5.0.3 on a PC with LNS already installed may not register the DRF kit for Xenta 100 correctly

Issue

Installing TAC Vista 5.0.3 on a PC with LNS already installed may not register the DRF kit for Xenta 100 correctly

If the DRF kit (Device Resource Files) is not correctly registered, it may not be possible to start the TAC XBuilder from TAC Vista.

Product Line

TAC Vista

Environment

  • TAC Vista 5.0.3
  • DRF Kit
  • XBuilder

Cause

LNS was previously installed on the PC before Vista was installed.

Resolution

Install ZBuilder standalone.