invalid data on _schedule address_ error when downloading application

Issue

"invalid data on _schedule address_" error when downloading application

Product Line

TAC Vista

Environment

  • Xenta Programmables
  • Xenta 280, 281, 282, 283, 300, 301, 302, 401, 401:B

Cause

This error can occur when the time schedule data has become corrupted in the Xenta programmable controller.

Resolution

To fix the controller either:

  1. Clear the MTA file by using the clear application process (see Lessons Learned Article #5143 for more information)
  2. Download the MOT file and empty the application memory (see Lessons Learned Article #4007 for more information).