Issue
Installing TAC Vista FM on a PC that does not have TAC Vista 5 installed.
Product Line
TAC Vista
Environment
- TAC Vista FM
- PC without TAC Vista 5
- Microsoft .NET Framework Version 2.0
- Microsoft Visual C++ 205 Redistributable
Cause
Microsoft assets must be installed prior to TAC Vista FM.
Resolution
To be able to run TAC Vista FM on a PC without having TAC Vista 5 installed, you will need to make sure that the PC has "Microsoft .NET Framework Version 2.0" and "Microsoft Visual C++ 2005 Redistributable" installed on the PC before you install TAC Vista FM.