Issue
SCU in double-address mode and the second station is not responding.
Once a card is read at any of the readers, a Reader Entry is displayed in the Transactions Window but the strike never fires.
The DO point can be manually controlled through Software but not by any of the readers.
Environment
- I/NET
- SCU1284
Cause
The MCU Configuration must be set to restore the DPU.
Resolution
- Connect to the controller, then go to MCU Configuration.
- Both of the addresses on the DPU should be Blue.
- Turn the second address to Internal and exit the editor.
- Open the Editor again and change the setting to DPU.
- Perform a DPU restore and try the card again.
- A Reader Entry should show up in the Transactions Window and the strike should fire, indicating that it is working properly.