Issue
How can you tell the difference between a I2/B3xxx -V and a I2/B3xxx controller through Continuum Explorer?
Environment
- I2/B3xxx
- I2/B3xxx -V
Cause
Determine the version of a controller remotely through Continuum Explorer
Resolution
- In Continuum Explorer, right click to edit a I2/B3xxx -V controller
- Select the runtime tab
-
Looking at the version of the controller is the way to distinguish between the different Models.
- The I2/B3xxx -V will have a version number similar to 3.501027
- A regular I2/B3xxx will have a number similar to 3.300006.
- Notice the location of the 1 in the -V version number. The -V models will have the 1 in the location as above while the non -V model will not.