Issue
ACWPPServerProxy applet is constantly flashing on webClient
Environment
- ACWPPServerProxy applet
- webClient
- Loopback
Cause
This typically happens on a Stand Alone configuration on Windows.
Resolution
The solution is to add the loopback address onto the IIS server by taking the following steps.
- Open IIS Manager
- Expand Web Sites> Right Click on Default Web Site and select Properties
- Click the Advanced button to the right of the IP address field
- Click the Add button and enter the IP: 127.0.0.1 and the port: 80, Click OK, OK
- Stop and Start IIS
- Launch Webclient and the ACWPPServerProxy applet will no longer flash.
- Restart the webclient PC
If you are using Windows 7, Vista or Windows Server 2008 the IIS interface is different.
- Open IIS Manager (the non 6.0 version) from Administrative Tools
- Expand Sites> Left click on Default Web Site
- In the far right column called Actions, locate the Bindings link
- Select Bindings and click the Add button then enter 127.0.0.1 into the IP address field (leave other defaults) Click Ok, Close
- With Default Web site still selection select "Restart" Under the Actions column to restart IIS
- Launch Webclient and the ACWPPServerProxy applet will no longer flash.
- Restart the webclient PC